This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/IWR1642BOOST: Use Indoor False Detection demo with IWR1642

Part Number: IWR1642BOOST
Other Parts Discussed in Thread: IWR1642, IWR6843, IWR6843ISK

Tool/software: Code Composer Studio

Hello TI,

Can I  use Indoor False detection with IWR1642Boost EVM , Is it Work...?

If yes, what Changes i need to for IWR1642 

Thanks,

Rahul

  • Hi Rahul,

    The Demos/Code examples released under SDK and/or TI Resource explorer mention which Device+Antenna board configurations these are developed for and are meant be used only with those.

    At this point the Classification demo example is made for IWR6843 device + ISK EVM board combination and will not work as -is on the IWR1642 device.

    In order to get equivalent functionality on the Classification component would have be retrained and implemented based on data from IWR1642 Device raw data. Please see the Algorithm information under the TIREx Lab to get a feel of various components inside the code.

    Thank you,
    Vaibhav
  • Hello Vaibhav,

    I try to calibrate IWR1642 for Indoor false detection but it not working
    by referring Programming Chirp Parameters in TI Radar Devices and indoor_false_det_68xx_chirp_parameters

    when i compare both code PPLCount and Indoor false detection, the only difference is classier present in Indoor false detection
    How to set configuration parameter for IWR1642
    what i need to do, I want avoid indoor false detection Plants, Curtains, Fan like Inanimate object



    Thanks,
    Rahul
  • Former Member
    0 Former Member in reply to Rahul Surawase48
    Hello Rahul,

    I believe this is similar to the request in this thread: e2e.ti.com/.../746522

    Please refer to the response here regarding support for the IFDM demo on IWR1642 - it is not supported. Please use an IWR6843ISK instead.

    Amanda