Working with a two electrode cell (with CE and RE shorted) I'm getting a consistent 400 Hz oscillation, only when the cell current is low (<10nA). Is the feedback circuit unstable at this low current or could it have to do with the geometry of the cell itself?
Is there anything I can do to improve the stability at very low currents?