This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RTOS/AWR1642BOOST: mmWave Visualizer no reaction after sending the configuration

Part Number: AWR1642BOOST


Tool/software: TI-RTOS

I flashed the suitable bin file to AWR1642BOOST Board successfully with 'Uniflsah'.

Then, I used the 'mmWave Demo Visualizer'  to run the demo. I chose suitable Setup parameters. However, when I click the 'SEND CONFIG TO MMWAVE DEVICE' Button, there is no reaction. Also, there is empty on the 'Console Messages' output. 

I am not sure of why this problem occurs, and if the board is wrong? Looking forward to your advice!

Thanks!

William