This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPT3001: OPT3001 is capable to handle 15KV ESD air strike ?

Part Number: OPT3001
Other Parts Discussed in Thread: STRIKE

One of my customer is using OPT3001 in one of  Product . Product level ESD requirement is 15kV (air) as per IEC61000-4-2.

Product plastic enclosure to PCB (component) distance only 3mm by air. What will happen ( Any damage to device ) if 15KV ESD strike is applied  during ESD test . Can device handle 15KV ESD strike. Since top portion of device is expose Optical part.