Other Parts Discussed in Thread: TDC7200
Hi Team,
We have penetrated our TDC1000+TDC7200 solution to my customer for detect of liquid level and concentration application. Now customer's board come back and is debugging on this, they met some question or issues that need expert to help support, thanks a lot!
Question 1. For TDC1000, how or when to select Short TOF and standard TOF? Do we have suggestions or guidelines for this;
Issue 1: If TDC use Standard TOF, TDC7200 use Mode 2, Ultrasonic driver frequency is 1MHz, TDC1000's TRIGG use rising edge, TDC7200's start and stop also use rising edge. Then if we use oscilloscope to monitor, the start and stop waveform is normal, but TDC7200's INTB didn't show sometimes. Do you have some idea why this happen?
Issue 2: If we still use 1MHz Ultrasonic driver frequency and TDC1000's TRIGG use rising edge, but TDC7200's start and stop use falling edge, then TDC7200's INTB will show normally. BTW, if we use 500kHz Ultrasonic driver frequency, TDC1000's TRIGG use rising edge, TDC7200's start and stop use rising edge, then the TDC7200's INTB will show normally, can you also help clarify why it is?
Issue 3: Now customer is using 1MHz Ultrasonic driver frequency, TDC1000 use rising edge, TDC7200's start and stop use falling edge, customer use 8MHz crystal(10ppm), the test result showed that these is about several nanosecond fluctuations or even tens of nanoseconds fluctuations sometimes, so do we have some solution or suggestions to improve this?
Thanks a lot for your great support on this!
Best regards,
Sulyn