Other Parts Discussed in Thread: AWR1642, , MMWAVE-STUDIO
Fig1 Fig2
I use mmwave studio 01_00_00_00+DCA1000+EVM of AWR1642 ES1.0/AWR1642 ES 2.0/AWR1243 ES2.0 to capture ADC data.
1/ When using mmwave studio, i found mmwave studio was always cannot output bin file from raw.bin file after capturing data by DCA1000. It crashes.
2/ When using these EVMs, i found mmwave -studio always tended to crash if i set a large number of frame, see fig1.
all above 2 cases, i have to restart mmwave studio, even re-power EVM.
As a result,I can only capture ADC data by restart, and capturing ADC data can not lasting a long time.
I know TI has mmwave studio 01_00_00_00 and 02_00_00_02. And each version of mmwave studio support different ES X.X.
My question are
1/ why mmwave studio can not output bin file from raw.bin? How to solve it?
2/ Why mmwave studio crashes easily when setting a large NUm of Frame? How can capturing data lasts a long time?
3/ Are these problems related to the version of mmwave studio?
Which version support AWR1642 ES1.0/AWR1642 ES 2.0/AWR1243 ES2.0? Maybe mmwave studio 1.0 support AWR1642 ES1.0, mmwave studio 2.0 support AWR1642 ES2.0,AWR1243 ES3.0
How about AWR1243 ES2.0?
4/ Sometime to save time,i capture data by getting several Raw.bin files and do not pres“postproc” button at the same time. So i do not get bin files immediately.
When i go back to office, i find i can not get bin file from Raw.bin file by using mmwave studio.
Is there any way to trans Raw.bin to bin file?