This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR1642BOOST: Error Running Lab Visualizer for People Counting

Part Number: IWR1642BOOST
Other Parts Discussed in Thread: UNIFLASH, IWR1642,

Dear,

When running the lab visualizer for the people counting, I receive the following message: 

Undefined variable "matlab" or class "matlab.webcam.internal.Utility.enumerateWebcams".

Error in webcamlist (line 25)

Error in setup>popupWebcam_CreateFcn (line 612)

Error in gui_mainfcn (line 95)

Error in setup (line 42)

Error in matlab.graphics.internal.figfile.FigFile/read>@(hObject,eventdata)setup('popupWebcam_CreateFcn',hObject,eventdata,guidata(hObject))

hObject =

UIControl (editUART) with properties:

Style: 'edit'
String: 'COM3'
BackgroundColor: [1 1 1]
Callback: [function_handle]
Value: 0
Position: [0.3046 0.7262 0.2831 0.2857]
Units: 'normalized'

Use GET to show all properties

Opening configuration file mmw_pplcount_demo_default.cfg ...
Sending configuration from mmw_pplcount_demo_default.cfg file to IWR16xx ...

Serial Port Object : Serial-COM3

Communication Settings
Port: COM3
BaudRate: 115200
Terminator: 'LF'

Communication State
Status: open
RecordStatus: off

Read/Write State
TransferStatus: idle
BytesAvailable: 0
ValuesReceived: 0
ValuesSent: 0


dfeDataOutputMode 1
Warning: Unexpected Warning: A timeout occurred before the Terminator was reached.
Warning: Unexpected Warning: A timeout occurred before the Terminator was reached.
Warning: Unsuccessful read: The specified amount of data was not returned within the Timeout period..
channelCfg 15 3 0

To explain what I have done so far, I am using IWR1642BOOST (not sure if it's ES1.0 or ES2.0). The label on the chip is "IWR1642  QG  82ZE3Y9  502AC  ABL  G1". Then, the used SDK is mmwave_industrial_toolbox_3_1_1. Lab011 has been successfully flashed using online UniFlash. Where is the issue?