This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Need Single IC for RTD(4-wire) & Thermocouple measurement with internal ADC, supporting I2C to communicate with controller

Other Parts Discussed in Thread: ADS122C04

Hi,

I am having a quite little experience in circuit design. I want to measure temperature, so i went for RTD (4-wire) & thermocouple options. I need an IC which can have an option for  RTD(4-wire) as well as thermocouple with internal ADC (so that I can avoid multiple ICs in the circuit ). The ADC is going to be connected to the micro controller which can support I2C only. So please could anyone recommend an IC that can fulfill my requirements.

thanking you in advance,

dwayne.

  • Hi Dwayne,

    Take a look at the ADS122C04. There are examples in the device datasheet showing circuits for both RTD and TC. You may need jumpers or switches to make it configurable for both sensors, but it is doable.

    Best regards,
    Bob B