This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR1642BOOST: confuse about the Er to design GCPW and antenna use RO4835 LoPro

Part Number: IWR1642BOOST


Hi experts:

     I'm confusing about the width of the GCPW, it is different between the roggers calculator and your documentation. roggers calculator's result is 8.74mil, but in the documentation is 7.08mil. In the documentation Er is 3.66, another documentation is 3.48, but roggers calculator shows Er is 3.461 at 78.5GHz. If I use Er 3.66 to calculate the width of the GCPW is about 7.08mil. 

    I want to know if I selected the wrong parameter of roggers calculator or which Er is correct? Which Er should I use to creat antenna and GCPW simulation in HFSS?

    The dielectric materials is RO4835 LoPro. 

 


Best regards!