Other Parts Discussed in Thread: TMP303, LM26NV
Could you recommend products for OUT pin remains high when the temperature is at or above the selected temperature threshold.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,Amit Ashara
YES,Because out pin rating only 4V for the TMP302,so I can't the high voltage pull low.
I need package is SOT563
Hi,Amit Ashara:
If choose TMP303 ,when the measured temperature is beyond the 125 °C or below the -15°C, the OUT pin is high?
I need only beyond the 125 °C the OUT pin is high.Could you recommend products?