Hi
Could you please answer the following questions?
1.
Beta compensation register is described in Table 10.
How to detect beta range automatically?
(What is monitored of the transistor?)
2.
In typical application of datasheet, the following sentence is described.
"Based on these criteria, two recommended small-signal transistors are the 2N3904 (NPN) or 2N3906 (PNP)."
And Figure 7 shows remote temperature error of 2N3906 with n-factor.
Does it mean that the calibration is not examined properly if other than these transistors are used?
BestRegards