This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

vital signs config for mmwave studio !

Other Parts Discussed in Thread: AWR1642, AWR1642BOOST

Hi all,

I am trying to apply the same vital signs configuration file into mmwave studio and get AWR1642 radar raw data as an output. I am a bit confused about the configuration that should take place in mmwave studio to record raw radar signals which allow me to g ofurther for a vital signs extraction from this raw data. 

my fisrtquestion is: should the signal be a complex signal or real signal ? because in the vitalsignslab config file, the adcCfg is: (2,1) which means that the signal should be complex one?  in mmwave studio log file, I have the equivalent config like this : AdcOutConfig (2,0,0), which means it is recording real signal!

my second question is about the ChannelConfig parameter: in vital signs lab, the ChannelCfg parameter is set to (15,3,0) which means using and 1 Tx and one Rx ? in mmwave studio,  from the log file, the channel conf parameters is: ChannelConfig,1,15,0.

and in the datacapturedemo.lua file, I am setting the channNadcConfig as follows: (1,0,0,1,1,1,1,2,0,0) which means using one tx, 4rx, single chirp, 16 bits,  and the (2,0,0) means that the signal to record is real!

I am confused between what the vitalsigns lab conf says, and when trying to apply it on mmwave studio, it seems to be not similar...

thanks in advance,

Ahmed

  • Ahmed,

    For your first question, the ADC output format is complex 1x. For your second question, all four RX antennas and both TX antennas are enabled. Only when we get to the actual chirp configuration do we specify the number of TX antennas that are turned on for the actual chirp.

    Please adjust these parameters to match your implementation in mmWave Studio.

    Regards,
    Kyle
  • Hi kyle,

    So the vital signs lab uses a complex 1x raw radar signals to extract the vital signs! Are they somehow mixed together (real and img parts of the signal) for the vital signs extraction?
    Thanks again for your response.

    Ahmed
  • kyle,

    attached, I uploaded the two conf files: the first for vital signs lab itself, and the second for the mmwave studio conf. I tried to adjust the first conf file parameters to match my implementation in mmWave Studio..

    can you take a look on it! am I missing something?

    thanks,

    Ahmed

    sensorStop
    flushCfg
    dfeDataOutputMode 1
    channelCfg 15 3 0
    adcCfg 2 1
    adcbufCfg -1 0 0 1 0
    profileCfg 0 77 7 6 57 0 0 70 1 200 4000 0 0 48
    chirpCfg 0 0 0 0 0 0 0 1
    frameCfg 0 0 2 0 50 1 0
    lowPower 0 0
    guiMonitor 0 0 0 0 1
    vitalSignsCfg 0.1 0.7 256 320 1 0.1 0.05 300000 300000
    motionDetection 1 40 0.02 0
    sensorStart
    
    
    

    --BSS and MSS firmware download
    info = debug.getinfo(1,'S');
    file_path = (info.source);
    file_path = string.gsub(file_path, "@","");
    file_path = string.gsub(file_path, "DataCaptureDemo_xWR.lua","");
    fw_path   = file_path.."..\\..\\rf_eval_firmware"
    
    --Export bit operation file
    bitopfile = file_path.."\\".."bitoperations.lua"
    dofile(bitopfile)
    
    --Read part ID
    res, efuserow9 = ar1.ReadRegister(0xffffe210, 0, 31)
    if (bit_and(efuserow9, 3) == 0) then
        partId = 1243
    elseif (bit_and(efuserow9, 3) == 1) then
        partId = 1443
    else
        partId = 1642
    end
    
    --ES version
    res, ESVersion = ar1.ReadRegister(0xFFFFE218, 0, 31)
    ESVersion = bit_and(ESVersion, 15)
    
    --ADC_Data file and Raw file and PacketReorder utitlity log file path
    data_path     = file_path.."..\\PostProc"
    adc_data_path = data_path.."\\adc_data.bin"
    Raw_data_path = data_path.."\\adc_data_Raw_0.bin"
    pkt_log_path  = data_path.."\\pktlogfile.txt"
    
    -- Download BSS Firmware(AR16xx)
    if((partId == 1642) and (ESVersion == 1)) then
        BSS_FW    = fw_path.."\\radarss\\xwr16xx_radarss_rprc_ES1.0.bin"
        MSS_FW    = fw_path.."\\masterss\\xwr16xx_masterss_rprc_ES1.0.bin"
    elseif((partId == 1642) and (ESVersion == 2)) then
        BSS_FW    = fw_path.."\\radarss\\xwr16xx_radarss_rprc_ES2.0.bin"
        MSS_FW    = fw_path.."\\masterss\\xwr16xx_masterss_rprc_ES2.0.bin"
    elseif((partId == 1243) and (ESVersion == 2)) then
        BSS_FW    = fw_path.."\\radarss\\xwr12xx_xwr14xx_radarss_ES2.0.bin"
        MSS_FW    = fw_path.."\\masterss\\xwr12xx_xwr14xx_masterss_ES2.0.bin"
    elseif((partId == 1243) and (ESVersion == 3)) then
        BSS_FW    = fw_path.."\\radarss\\xwr12xx_xwr14xx_radarss_ES3.0.bin"
        MSS_FW    = fw_path.."\\masterss\\xwr12xx_xwr14xx_masterss_ES3.0.bin"
    elseif((partId == 1443) and (ESVersion == 2)) then
        BSS_FW    = fw_path.."\\radarss\\xwr12xx_xwr14xx_radarss_ES2.0.bin"
        MSS_FW    = fw_path.."\\masterss\\xwr12xx_xwr14xx_masterss_ES2.0.bin"
    elseif((partId == 1443) and (ESVersion == 3))then
        BSS_FW    = fw_path.."\\radarss\\xwr12xx_xwr14xx_radarss_ES3.0.bin"
        MSS_FW    = fw_path.."\\masterss\\xwr12xx_xwr14xx_masterss_ES3.0.bin"
    else
        WriteToLog("Inavlid Device partId FW\n" ..partId)
        WriteToLog("Inavlid Device ESVersion\n" ..ESVersion)
    end
    
    -- Download BSS Firmware(AR16xx)
    if (ar1.DownloadBSSFw(BSS_FW) == 0) then
        WriteToLog("BSS FW Download Success\n", "green")
    else
        WriteToLog("BSS FW Download failure\n", "red")
    end
    RSTD.Sleep(2000)
    
    -- Download MSS Firmware
    if (ar1.DownloadMSSFw(MSS_FW) == 0) then
        WriteToLog("MSS FW Download Success\n", "green")
    else
        WriteToLog("MSS FW Download failure\n", "red")
    end
    RSTD.Sleep(2000)
    
    -- SPI Connect
    if (ar1.PowerOn(1, 1000, 0, 0) == 0) then
        WriteToLog("Power On Success\n", "green")
    else
       WriteToLog("Power On failure\n", "red")
    end
    RSTD.Sleep(1000)
    
    -- RF Power UP
    if (ar1.RfEnable() == 0) then
        WriteToLog("RF Enable Success\n", "green")
    else
        WriteToLog("RF Enable failure\n", "red")
    end
    RSTD.Sleep(1000)
    
    if (ar1.ChanNAdcConfig(1, 0, 0, 1, 1, 1, 1, 2, 0, 0) == 0) then    -- 1 tx, 4 rx, single chip, 16 bit, complex 1x (1 / real data (0), I signal first
        WriteToLog("ChanNAdcConfig Success\n", "green")
    else
        WriteToLog("ChanNAdcConfig failure\n", "red")
    end
    RSTD.Sleep(1000)
    
    if (partId == 1642) then
        if (ar1.LPModConfig(0, 0) == 0) then           -- Low Power ADC (0,1)
            WriteToLog("LPModConfig Success\n", "green")
        else
            WriteToLog("LPModConfig failure\n", "red")
        end
    else
        if (ar1.LPModConfig(0, 0) == 0) then           -- Regular ADC (0,0)
            WriteToLog("Regualar mode Cfg Success\n", "green")
        else
            WriteToLog("Regualar mode Cfg failure\n", "red")
        end
    end
    RSTD.Sleep(2000)
    
    if (ar1.RfInit() == 0) then
        WriteToLog("RfInit Success\n", "green")
    else
        WriteToLog("RfInit failure\n", "red")
    end
    RSTD.Sleep(1000)
    
    if (ar1.DataPathConfig(1, 1, 0) == 0) then            -- LVDS , ADC only, packet 1 / suppress packet
        WriteToLog("DataPathConfig Success\n", "green")
    else
        WriteToLog("DataPathConfig failure\n", "red")
    end
    RSTD.Sleep(1000)
    
    if (ar1.LvdsClkConfig(1, 1) == 0) then                --- DDR clock, data rate: 600Mbps
        WriteToLog("LvdsClkConfig Success\n", "green")
    else
        WriteToLog("LvdsClkConfig failure\n", "red")
    end
    RSTD.Sleep(1000)
    
    if(partId == 1642) then
        if (ar1.LVDSLaneConfig(0, 1, 1, 0, 0, 1, 0, 0) == 0) then      -- Lne format 0, lane 1, lane 2 , MSB first, 
            WriteToLog("LVDSLaneConfig Success\n", "green")
        else
            WriteToLog("LVDSLaneConfig failure\n", "red")
        end
    elseif ((partId == 1243) or (partId == 1443)) then
        if (ar1.LVDSLaneConfig(0, 1, 1, 1, 1, 1, 0, 0) == 0) then
            WriteToLog("LVDSLaneConfig Success\n", "green")
        else
            WriteToLog("LVDSLaneConfig failure\n", "red")
        end
    end
    RSTD.Sleep(1000)
    
    if(partId == 1642) then
        if(ar1.ProfileConfig(0, 77, 7.01, 6, 57, 0, 0, 0, 0, 0, 0, 70.106, 1, 200, 4000, 0, 0, 48) == 0) then  --ar1.ProfileConfig(0, 77, 7.01, 6, 57, 0, 0, 0, 0, 0, 0, 70.006, 1, 100, 2000, 0, 0, 40)
    
            WriteToLog("ProfileConfig Success\n", "green")
        else
            WriteToLog("ProfileConfig failure\n", "red")
        end
    elseif((partId == 1243) or (partId == 1443)) then
        if(ar1.ProfileConfig(0, 77, 100, 6, 60, 0, 0, 0, 0, 0, 0, 29.982, 0, 256, 10000, 0, 0, 30) == 0) then
            WriteToLog("ProfileConfig Success\n", "green")
        else
            WriteToLog("ProfileConfig failure\n", "red")
        end
    end
    RSTD.Sleep(1000)
    
    if (ar1.ChirpConfig(0, 0, 0, 0, 0, 0, 0, 1, 0, 0) == 0) then       -- TX0, TX1
        WriteToLog("ChirpConfig Success\n", "green")
    else
        WriteToLog("ChirpConfig failure\n", "red")
    end
    RSTD.Sleep(1000)
    
    if (ar1.FrameConfig(0, 0, 36000 , 2 , 50 , 0 , 1) == 0) then      -- 8 frames, 128 chirps, periodicity: 40 ms, software trigger(1)
        WriteToLog("FrameConfig Success\n", "green")
    else
        WriteToLog("FrameConfig failure\n", "red")
    end
    RSTD.Sleep(2000)
    
    -- select Device type
    if (ar1.SelectCaptureDevice("DCA1000") == 0) then
        WriteToLog("SelectCaptureDevice Success\n", "green")
    else
        WriteToLog("SelectCaptureDevice failure\n", "red")
    end
    RSTD.Sleep(1000)
    
    --DATA CAPTURE CARD API
    if (ar1.CaptureCardConfig_EthInit("192.168.33.30", "192.168.33.180", "12:34:56:78:90:12", 4096, 4098) == 0) then
        WriteToLog("CaptureCardConfig_EthInit Success\n", "green")
    else
        WriteToLog("CaptureCardConfig_EthInit failure\n", "red")
    end
    RSTD.Sleep(1000)
    
    --AR12xx or AR14xx-1, AR16xx- 2 (second parameter indicates the device type)
    if (partId == 1642) then
        if (ar1.CaptureCardConfig_Mode(1, 2, 1, 2, 3, 30) == 0) then
            WriteToLog("CaptureCardConfig_Mode Success\n", "green")
        else
            WriteToLog("CaptureCardConfig_Mode failure\n", "red")
        end
    elseif ((partId == 1243) or (partId == 1443)) then
        if (ar1.CaptureCardConfig_Mode(1, 1, 1, 2, 3, 30) == 0) then
            WriteToLog("CaptureCardConfig_Mode Success\n", "green")
        else
            WriteToLog("CaptureCardConfig_Mode failure\n", "red")
        end
    end
    RSTD.Sleep(1000)
    
    if (ar1.CaptureCardConfig_PacketDelay(25) == 0) then
        WriteToLog("CaptureCardConfig_PacketDelay Success\n", "green")
    else
        WriteToLog("CaptureCardConfig_PacketDelay failure\n", "red")
    end
    RSTD.Sleep(1000)
    
    --Start Record ADC data
    ar1.CaptureCardConfig_StartRecord(adc_data_path, 1)
    RSTD.Sleep(1000)
    
    --Trigger frame
    ar1.StartFrame()
    RSTD.Sleep(1800000)
    
    --Packet reorder utility processing the Raw_ADC_data
    WriteToLog("Please wait for a few seconds for Packet reorder utility processing .....!!!! \n", "green")
    ar1.PacketReorderZeroFill(Raw_data_path, adc_data_path, pkt_log_path)
    RSTD.Sleep(4000)
    WriteToLog("Packet reorder utility processing done.....!!!! \n", "green")
    
    --Post process the Capture RAW ADC data
    ar1.StartMatlabPostProc(adc_data_path)
    --writeToLog("Please wait for a few seconds for matlab post processing .....!!!! \n", "green")
    RSTD.Sleep(4000)
    

  • Kyle,
    concerning the first question, in the complex 1x data mode, what does each part of the signal means ! real signal is the transmitted ! and img signal is the received !
    thanks,
    Ahmed
  • Ahmed,

    This understanding is not correct. Please refer to this previous E2E thread about understanding the difference between complex 1x mode and complex 2x mode.



    Please keep in mind that the vital signs extraction is done on the DSP of the AWR1642BOOST EVM. It is not just the raw signal itself that gives the vital signs information. This is achieved primarily in software and not in hardware. Attempting to use mmWave Studio and just copy the profile configuration from the vital signs demo is only one aspect of this lab. I would suggest reading through the User's Guide that is included for this lab to get a better understanding of how this lab actually works. All of the source code for this lab is provided on TI's Resource Explorer.

    Regards,
    Kyle