Other Parts Discussed in Thread: TMP102, ,
Hello there,
I am working on a custom two layer PCB board interfacing the OPT3101 IC with my PIC18F452 8-bit microcontroller from Microchip. My controller is communicating correctly with the OPT3101 IC. The issue is that i don't have the availability of a 12-bit external temperature sensor like TI's TMP102 sensor as used in the OPT3101 Evaluation Module for phase corrections since i'm trying to replicate the design of the EVM module in my custom board.
I have a 10-bit temperature sensor available i.e. AD7414 from Analog Devices which also communicates in I2C protocol, same as TMP102. Is there any way to use my 10 bit temperature sensor with the OPT3101 IC since it only expects either 12-bit or 8-bit temperature data as mentioned in the datasheet?
Best Regards,
Rummaan Bin Amir