This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1243BOOST: What is the maximum length of the cable between the MMWAVE-DEVPACK board and the TSW1400

Part Number: AWR1243BOOST

Can you let me know the the maximum length of the cable (HQCD-XXX-08.00-TBL-SBR-1-D) between the MMWAVE-DEVPACK board and the TSW1400?

We are looking to use a cable length of 20" to 30" and want to know if this is OK?