This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR6843: IWR6843 firmware files for OOB demo / ROS

Part Number: IWR6843


Greetings! 

I'm trying to get the ROS CLOUD ( lab006 ) going for 6843.    Have trouble  flashing the  .bin files .   Tried 2 boards and different computers ( WIndows) ..Could repeat the error .

Using SDK3_0_0_8: 

Flash Image(s)
check_box Meta Image 1
 iwr6xxx_radarss_rprc.binSize: 212.19 KB
 Browse 
check_box Meta Image 2
 xwr68xx_mmw_demo.binSize: 338.57 KB
 Browse
 

[11/29/2018, 3:08:20 PM] [INFO] Cortex_R4_0: Initialization complete.
[11/29/2018, 3:08:20 PM] [INFO] Cortex_R4_0: Flashing process starting...
[11/29/2018, 3:08:20 PM] [INFO] Cortex_R4_0: Connecting to COM Port COM4...
[11/29/2018, 3:08:20 PM] [INFO] Cortex_R4_0: Reset connection to device
[11/29/2018, 3:08:20 PM] [INFO] Cortex_R4_0: Set break signal
[11/29/2018, 3:08:20 PM] [INFO] Cortex_R4_0: Connection to COM port succeeded. Flashing can proceed.
[11/29/2018, 3:08:20 PM] [INFO] Cortex_R4_0: Reading device version info...
[11/29/2018, 3:08:20 PM] [INFO] Cortex_R4_0: ** 2 files specified for flashing.
[11/29/2018, 3:08:20 PM] [INFO] Cortex_R4_0: Checking file C:/ti/mmwave_sdk_03_00_00_08/firmware/radarss/iwr6xxx_radarss_rprc.bin for correct header for IWR6843.
[11/29/2018, 3:08:20 PM] [INFO] Cortex_R4_0: Header of C:/ti/mmwave_sdk_03_00_00_08/firmware/radarss/iwr6xxx_radarss_rprc.bin file indicates it is not a valid file to flash to IWR6843: 0x43525052
[11/29/2018, 3:08:20 PM] [ERROR] Cortex_R4_0: !!! Aborting flashing of specified files!!!
[11/29/2018, 3:08:20 PM] [INFO] Cortex_R4_0: Disconnecting from device on COM port COM4...
[11/29/2018, 3:08:20 PM] [INFO] Cortex_R4_0: Flashing instance clean-up initiated...
[11/29/2018, 3:08:20 PM] [INFO] Cortex_R4_0: Instance deinitialized!
Appreciate  a quick resolution and fix 
thanks 
...ravi
  • Hello Ravi,

    Please see the "How do I Re-flash the TI mmWave EVM with Out-of-Box demo?" section in the ROS Point Cloud Visualizer lab setup guide. On page 18 it mentions the image to flash:

    9. Specify the following flash image:
    For xWR6843 EVM:
    Meta Image 1:
    {$MMWAVE_SDK_INSTALL_DIR}/packages/ti/demo/{$YOUR_DEVICE}/mmw/xwr68xx_mmw
    _demo.bin

    Please note that IWR6843 only needs a single bin file to be flashed since the bin file includes both the MSS and RadarSS images.

    Regards,
    John
  • John 

    Oops, my bad... I was looking @ version 1.4 of doc and followed  the guidelines there f for new 6843. 

    This works now 

    thanks 

    ...ravi