Hello ,
I have bought ARW1243 (Ver.E2.0),and useDCA 1000 to test the board ARW1243 boost in both mmwave studio 1.0 and 2.0.
there are several bugs:
1) SPI connect
10:10:43] [RadarAPI]: ar1.PowerOn(0, 1000, 0, 0)
10:10:43] Status: Failed, Error Type: RESP TIMEOUT
LUA shows PowerOn failure
2) some time SPI connect is OK but RF power is down
the function is ar1.RfEnable() LUA shows ans= -8
and I can't get through this bug
I use two separate 5V2A DC power and SOP0/1 is closed with Jumpers
and other questions:
1) what's the difference between mmwave studio 1.0 and 2.0 's firmware? version numis the same is BSS FW
2) Can I use mmwave studio 2.0 to develop ARW1243 (Ver.E2.0)?
3 )can these bugs be solved ? if not ,can I return the board or change to the new verison ?
thank you for your time and consideration !
best regards !
Allen