Dear Sir/Madam,
I have a few question regarding the datasheet and the sample design:
1- in page 105 from datasheet how do you come up with the equation 11. What is the number 30 in the numerator and denominator of this equation? 30/(30+C_PD)?
2- For the sample design using OSRAM SFH4550 LED mentioned in page 103 of the datasheet, in order to have 64mW radiant power in the FOV, we need to have 7.4W/sr intensity from the LED. This is only possible if the peak driving current of the LED be around 670mA. So my question is: Is the maximum rating for I_DRV=173.6mA at page 6 related to an average driving current or it is the maximum available peak current from the chip in pulsed condition? If it is the pulsed peak current then do we need an external power supply for LED?
3- Is there any limitations for the rise/fall time of the LED?
4- in page 18, equation 4, how do you derive the second equality? What do you mean by BW signal measurement bandwidth?
Thank you in advance.
Kind regards,
Mehdi