This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR6843: detection angle

Part Number: IWR6843


Thank you for the provided info and links.

What is the angle in degree the sensor as such can be used to detect goods on a shelf. Or in other words, when i want to detect product standing in line for 50 cm, which height i need to detect all products on this 50 cm lined up? I read somewhere 120 degree - but i am not sure about.

Thanks

  • Hi Juergen,

    Here are the FOV (Field of View) specs for the IWR6843 ISK (Standard Antenna Plug-in Module):

    Azimuth i.e. Horizontal FOV: 110 degrees (i.e. +/- 55 degrees)

    Elevation i.e. Vertical FOV: 40 degrees (i.e. +/- 20 degrees)

    The above FOV is defined based on 6dB drop in the signal peak as compared to bore-sight or zero degrees. Note that the FOV is dependent upon the Antenna design and a different antenna design can have different FOV (narrower or wider). We also have an Antenna Database under mmWave Industrial Toolbox which is a repository of all the antenna designs put together by the TI mmWave Team.

    Please mark this thread resolved if your question was answered otherwise get back if you have more questions on this topic.

    Regards

    -Nitin