A related question is a question created from another question. When the related question is created, it will be automatically linked to the original question.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Choosing the right DSP + Evaluationboard for Sensorapplication
You would need an external ADC to do sensing at 24-bit resolution, but auxiliary inputs can be done via on-chip ADC (12-bit or 16-bit). 24-bit outputs would need to be via external EVM, but auxiliary outputs can be achieved via a 12-bit DAC or PWM module.
If you needed more processing power, you might look at the Beagle Bone (https://beagleboard.org/bone). This would be able to directly mate with an external EVM if it was in 'cape' format.
Is it possible to extend one of the Evaluation Kits /Board below with those 24-bit ADC (maybe with Codecs)
Best Regards
Viktor Heinz
Gesendet: Mittwoch, 05. Dezember 2018 um 21:26 Uhr Von: "Devin Cottier" <bounce-1120590@mail.e2e.ti.com> An: mmwave_sensors_forum@mail.e2e.ti.com Betreff: Sensors forum: Choosing the right DSP Evaluationboard for Sensorapplication
You would need an external ADC to do sensing at 24-bit resolution, but auxiliary inputs can be done via on-chip ADC (12-bit or 16-bit). 24-bit outputs would need to be via external EVM, but auxiliary outputs can be achieved via a 12-bit DAC or PWM module.
If you needed more processing power, you might look at the Beagle Bone (https://beagleboard.org/bone). This would be able to directly mate with an external EVM if it was in 'cape' format.
Did a reply answer your question? If yes, please click the "Resolved" button located at the bottom of that post. Visit these helpful C2000 Links!