Other Parts Discussed in Thread: MSP-FET
Hello,
i already asked a question like this and one of the supports (James Evans) did a great job. But i am at the point, where i dont get further with his explanation. Maybe if some different person can explain it to me, i will understand it.
Currently i got the MSP-FET Debugger and the FDC2214-EVM. In order to programm the FDC2214EVM with a MSP430-F5529 on it, i need to connect the debugger with jumper wires to the FDC. I already understood to connect J9 of the FDC with TDO and TCK of the Debugger. I also need to connect my J2 of the debugger with VCC Tool. James also told me to connect J3.11 and J3.13 with spots on the MSP-Fet. But that is the point, where i dont get further. Where do i connect these 2 on the MSP-Fet? Are there any other connections i need to do? A visual plan would maybe help me a lot. Or just the connections like J3.13(FDC)-->J2(MSP-FET) for example.
Thanks,
Marius