This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR6843: IWR6843 for SIL2 application

Part Number: IWR6843

Hi all,

in the datasheet of the IWR6843 was written that this chip is SIL2 Targeted. What it means?

Do you include or do you plan to add in the future a lockstep architecture for one or for both of the inside processors (DSP or ARM)?

I see that the chip has a lot of feature that can be used to identify a failure of some parts of it but to have a complete SIL2 system you need also that the processing has to be made in a lockstep architecture.

Thank you.

Alessandro.