This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/IWR1443BOOST: Trying the Vital Sign Lab. Everything goes well until the final step: running the Matlab GUI.

Part Number: IWR1443BOOST
Other Parts Discussed in Thread: UNIFLASH

Tool/software: Code Composer Studio

After I ran the VitalSignsDemo_GUI, I got the following errors. Can you help???

[Cortex_R4_0] **********************************************

Debug: Launching the Vital Signs Measurements Demo
**********************************************
Debug: Launched the Initialization Task
Debug: HWA has been initialized
Debug: EDMA instance 0 has been initialized
Debug: UART Instance @08009940 has been opened successfully
Debug: UART Instance @0800994c has been opened successfully
Debug: mmWave Control Initialization was successful
Debug: mmWave Control Synchronization was successful
Debug: CLI is operational
Debug: Start ADCBuf driver dataFormat=0, sampleSwap=1, interleave=0, chirpThreshold=1
Error: HWA_configParamSet(4) returned -2801 in function HWAutil_configVitalSignsFFT
Exception occurred in ThreadType_Task.
Task handle: 0x8003778.
Task stack base: 0x80037c8.
Task stack size: 0xc00.
R0 = 0x5105fffc R8 = 0x080082c4
R1 = 0x0000fbff R9 = 0x080082c4
R2 = 0x08004010 R10 = 0x510217d0
R3 = 0x080088c8 R11 = 0xffffffff
R4 = 0x00000000 R12 = 0x00000000
R5 = 0x00000000 SP(R13) = 0x08003fc0
R6 = 0x7ec51bde LR(R14) = 0x000003ff
R7 = 0x00000000 PC(R15) = 0x0000afa4
PSR = 0x200c019f
DFSR = 0x00000008 IFSR = 0x00000000
DFAR = 0x51060000 IFAR = 0x00000000
{module#40}: line 205: error {id:0x180000, args:[0xafa4, 0x3ff]}
xdc.runtime.Error.raise: terminating execution