This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1443BOOST: How to understand the serial data?

Part Number: AWR1443BOOST

Hi,

I have data in the following format:

Packet ID: 3722
Version: 1020005
TLV: 3
Detect Obj: 6
Platform: A1642
Subframe: 0
Detect Obj: 6
ObjId: 0
DopplerIdx: 0
RangeIdx: 1
PeakVal: 723
X: -00.043
Y: 000.000
Z: 000.000
Range: 000.043m
ObjId: 1
DopplerIdx: 0
RangeIdx: 41
PeakVal: 3659
X: -00.111
Y: 001.785
Z: 000.000
Range: 001.789m
ObjId: 2
DopplerIdx: 0
RangeIdx: 51
PeakVal: 6107
X: 001.182
Y: 001.885
Z: 000.000
Range: 002.225m
ObjId: 3
DopplerIdx: 0
RangeIdx: 255
PeakVal: 46
X: 005.215
Y: 009.828
Z: 000.000
Range: 011.126m
ObjId: 4
DopplerIdx: 1
RangeIdx: 18
PeakVal: 112
X: -00.639
Y: 000.457
Z: 000.000
Range: 000.785m
ObjId: 5
DopplerIdx: 0
RangeIdx: 255
PeakVal: 40
X: -04.172
Y: 010.312
Z: 000.000
Range: 011.124m
RangeProf[0]: 091.787
RangeProf[1]: 099.316
RangeProf[2]: 097.093

Can someone tell me what each of these things means? thanks.

  • Hi,

    Can you please go through the demo documentation available in "C:\ti\mmwave_sdk_01_02_00_05\packages\ti\demo\xwr14xx\mmw\docs\doxygen\html\index.html " ?

    This should cover each of these terms.

    If you still have questions, please raise a separate thread and we will assist.

    Best Regards,
    Anand