Other Parts Discussed in Thread: IWR1443
Tool/software: TI-RTOS
Hi,
I'm looking to migrating vital sign demo to sdk 2.1 for AWR1443 ES3.0 platform. Please point me changes needs to be done.
Reference sources from SDK 1.2:
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Madan,
The IWR1443 Vital Signs lab currently only supports IWR1443 ES2.0 (and corresponding mmWave SDK 1.2.0.5). It will be ported to ES3.0 (and corresponding mmWave SDK 2.1.0.4) in one of the future Industrial Toolbox releases (specific release date is not available at this time).
Here are the steps we will likely follow to port the current IWR1443 Vital Signs lab to mmWave SDK 2.1.0.4 for IWR1443 ES3.0. You are welcome to try it yourself in the meantime if desired.
1. Compare the latest 1443 OOB demo lab projectspec which supports mmWave SDK 2.1.0.4 to the projectspec in the previous version of that lab from Industrial Toolbox v2.5.2 (which supported mmWave SDK 1.2.0.5) and then make the same type of changes to current Vital Signs projectspec
2. Compare the 1443 OOB demo source code from mmWave SDK 2.1.0.4 to the source code in mmWave SDK 1.2.0.5 and then make the same type of changes to current IWR1443 Vital Signs source code as needed
3. Import the newly created IWR1443 Vital Signs Lab projectspec and build the project
Please note the following important differences between IWR1443 ES2.0 and ES3.0:
Please mark this thread resolved if your question was answered.
Regards,
-Nitin