This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

HDC2010: Issues when address pin is tied high

Part Number: HDC2010

The sensor doesn't seem to acknowledge I2C communications when its address pin is tied high and software I2C with the address 0x41.  With the address pin tied to ground and a software I2C address of 0x40, it works.  It has been powered at 3 V and 3.3V with the same results. 

If I could, I would change the address pin connection, but the hardware I have has the address pin tied to VDD.  What am I missing?