In the serial data, we see some terms like this:
RangeProf[0]: 091.787
RangeProf[1]: 099.316
RangeProf[2]: 097.093
RangeProf[3]: 091.389
RangeProf[4]: 086.496
What do they mean?
I asked a question and got the following answer...
"The values represent the signal strength/relative power for the given range bin index. For example, you would interpret RangeProf[4]: 086.496 as at the 4th range bin the relative power was 86.496 dB. This array of data is what comprises the Range Profile plot shown in the Demo Visualizer."
I would like to know what is this power relative to?