Hi everyone
I'm testing our custom board built-in OPT3101.
I measured the distance up to 5M but accuracy is not exactly.
I only connected I2C line between opt3101 and our custom board.
I don't use the external temperature sensor and external clock.
To improve the accuracy, must use the external clock?
Currently, opt3101 register value is same with OPT3101-EVM.
The efm32 MCU, our custom board MCU, don't have the clock pins. it has the only clock input pins for an external crystal.
If I use the GP2, which pin is connected with OPT3101.
It is a very hot place which our application is set. Maybe over the 100 degrees.
In this environment, for measuring accuracy I have to apply the external clock and external temperature?
Best Regards