This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPT8241-CDK-EVM: How many OPT8241-CDK-EVM can be operated by one PC concurrently?

Part Number: OPT8241-CDK-EVM

Hi,

I'm trying to work with multiple modules(4~5). I found the post where some people could work with two modules simultaneously.

How many modules can be operated at the same time by a single PC? If I'd like to work with 4~5 modules, is it recommended to connect them to two or three PCs?

Thanks

  • Jongho,

    This depends on the USB capability of your PC. It runs on bulk end point (data transfer mode for USB). Transactions taking place at the same time can cause data transfer to get delayed. Delay in data transfer can cause frame drops.
    So we have not checked for more than 1 camera on a PC. However, depending on your PC, and the kind of devices connected on your computer, it could handle more cameras. We have not made many modules work on 1 PC so I would recommend that you use multiple PCs for your evaluation.

    Regards,
    Subhash