Part Number: TDC1000-TDC7200EVM
We have a meter body with two 4MHz transducers facing each other between 2-5.5 inches.
We are looking for a replacement ultrasonic chip set.
The question I have is is the TDC1000-TDC7200EVM able to handle two transducers?
One transducer on one channel is set for send/start and the other transducer is on the other channel for receive/stop.
Then the process is reversed to compare the upstream/downstream rates.
Is this something that can be done with the TDC1000-TDC7200EVM?
Can it be done with the current GUI? I have no idea how to set up the various parameters, so any assistance will be appreciated. Thus far all my efforts have resulted in ... nothing.
Wade