Other Parts Discussed in Thread: UNIFLASH, , IWR6843
I'm experiencing an intermittent problem with UniFlash and IWR6843ISK in which UniFlash becomes unresponsive when trying to connect to the COM port. Some times UniFlash works correctly when programming this board so I know the COM port setting is correct, but other times when I try to load the firmware UniFlash just locks up trying to connect to the COM port (screen shot below). Also when this happens I can close UniFlash, but the COM port is still being held by the driver and I am not able to connect to it with Teraterm or subsequent UniFlash sessions. We have confirmed this behavior with multiple IWR6843ISK boards. Is this a known problem or is anyone experiencing something like this? Workarounds to avoid it?
I am using a Dell E7450 laptop running Windows 7 pro and natively installed UniFlash v4.5.0.2056. Another team member here confirmed similar behavior with the cloud based UniFlash.