Other Parts Discussed in Thread: AWR1642, DCA1000EVM, MMWAVE-SDK
Hi, I am going to use AWR1642 BOOST for autonomous application research.
Data transmission to the host PC of car from radar would be done with ethernet communication.
Data could be an 1-D or 2-D FFT result or object X,Y data.
And I would use Demo file or SRR demo file for radar.
Is it possible to use UART to Ethernet converter for AWR1642 EVM board to transmit those data(FFT,Raw,object X,Y) to PC?
Or do i have to use DCA1000EVM for it?
And is there any parsing code or data transmit format for those data?
I would be appreciate if there is any answer for them
Thanks for reading