Other Parts Discussed in Thread: MSP-EXP430F5529LP,
Hello team,
Customer is currently evaluating the EVM (MSP-EXP430F5529LP + BOOSTXL-PGA460). The customer's sensor at transmitter side has 42.4Vp-p(+21.1Vp, -21.1Vp) specification.
1-1. The transmitter sensor is applied 120Vp-p (+60Vp, -60Vp) voltage because of Vpwr=7.5V and transformer=1:1:8.42. If OUTB XD1 (Pin#:T1-1) is open, the voltage which the transmitter sensor is applied is in half of 120Vp-p (60Vp-p)? If yes, is there any problem with using OUTB=Open?
1-2. If OUTB is not used, what is the recommended termination for this pin? (NC, tie to GND or pull-down/up?)
1-3. In above case of 1-1, the test result was that the voltage was -30V <=> +30V swing, not 0V <=> +60V swing. Is this behavior correct? Could you let us know the mechanism for +/-30V swing in case of 1-1 (OUB=Open)?
2-1. The customer would like to use the transformer with 2.5V center-tap, but the center-tap is connected with Vpwr on the EVM. Can the customer cut the center-tap connection to Vpwr(min.6V) and newly connect with 2.5V? Is there any problem with changing the center-tap voltage from Vpwr on EVM to 2.5V?
3-1. Could you provide the recommended 1:1:3 transformer?
4-1. If a transformer is not used and full-bridge circuit at MA40H1S-R side is used, we think below component change is needed. Is that correct?
R30: Not mounted => Add 1kohm resistor
R35: 0ohm resistor => Not mounted
R34: Not mounted => Add 0ohm resistor
Regards,
Ishida