This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPT3006: Can OPT3006 powered from 1.8V

Part Number: OPT3006

Hi,

We are using OPT3006 as the Ambient light sensor and we like to use 1.8 V as the supply to the sensor. Can I use the 1.8V as power supply and connect the pins of the sensor to a host device with 1.8V as the pin voltage? Will it work properly?