Other Parts Discussed in Thread: UNIFLASH, AWR1642
Tool/software: Code Composer Studio
Hi,
1. I am using the "Object Data Over CAN"
2. After UniFlash debug image, dss and mss rebuild, target launch the AWR1632BOOST board start sending data through the CAN bus.
I can see CAN_H and CAN_L in the oscilloscope.
3. If I run the TI CAN Visualizer, the AWR1642 stops sending data and I have to restart the board and to launch the target again
4. The shortest bits I've seen in the oscilloscope are about 200ns (5M bps)
5.How can I change the baud rate to 1M bps in the mms code?
My CAN-USB adapter support this baud rate.
6. I will be glad to receive advices from anyone thas has faced the same problem.
Thank you.
Claudio
Thanks,
Claudio