This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR1642BOOST: Connection to mmwave Studio

Part Number: IWR1642BOOST
Other Parts Discussed in Thread: IWR1642

Hello, 

currently i am Using the IWR1642BOOST to get in common with Radar Technologies. I'd also like to Change chirp Scene Parameters and get a bit deeper in possibilities to Change behaviour. I read about th mmwave SDK and installed the mmwaveStudio. 

To connect my IWR1642 with the mmwave Studio do I Need any additional board or is it enough with the IWR1642 connected to PC via microUSB ? 

thanks for your help