Other Parts Discussed in Thread: IWR6843, IWR1642BOOST
Hi
I'm trying to implement people count demo on AWR1642BOOST-ODS. I made following modification on chirp config :
- "channelCfg 3 3 0" to activate RX1, RX2, TX1 and TX2, this makes a virtual antenna array of size 4 which is allowed by the demo
-
"SceneryParam 0 3 0.05 4" I put the board on the corner of my room
-
"AllocationParam 10 0.01 15 1 2" due to lower antenna gain on AWR1642BOOST-ODS I decreased minimum total SNR to 10 and minimum number of points to 15
Then I ran the demo , it gave me a rich point cloud on visualizer when I walked in front of it but it didn't assign any track. Please tell me how to configure chirp configuration to make it work on AWR1642BOOST-ODS.
Regards
Hossein