This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR1443BOOST: I cant program IWR1443BOOST with any demo like High Accuracy Range Measurement by UniFlash

Part Number: IWR1443BOOST
Other Parts Discussed in Thread: AWR1642BOOST, AWR1642, IWR1443, MMWAVE-SDK

Hi,

I have just started to explore TI mmWave devices, so I just started working with AWR1642BOOST and IWR1443BOOST.

With AWR1642 I could run diffrent demos but with IWR1443BOOST I couldn't program any file on its flash memory.

For example when I try to program  High Accuracy Range Measurement demo and files  xwr12xx_xwr14xx_radarss.bin file in the \firmware\radarss folder

and xwr14xx_mmw_demo_mss.bin in the \packages\ti\demo\xwr14xx\mmw folder, I get following errors:

[18.12.2018, 14.45.17] [INFO] Cortex_R4_0: Reset connection to device
[18.12.2018, 14.45.17] [INFO] Cortex_R4_0: Set break signal
[18.12.2018, 14.45.17] [INFO] Cortex_R4_0: Connection to COM port succeeded. Flashing can proceed.
[18.12.2018, 14.45.17] [INFO] Cortex_R4_0: Reading device version info...
[18.12.2018, 14.45.17] [INFO] Cortex_R4_0: ** 2 files specified for flashing.
[18.12.2018, 14.45.17] [INFO] Cortex_R4_0: Checking file C:/ti/mmwave_sdk_01_02_00_05/firmware/radarss/xwr12xx_xwr14xx_radarss.bin for correct header for IWR1443.
[18.12.2018, 14.45.17] [INFO] Cortex_R4_0: Header of C:/ti/mmwave_sdk_01_02_00_05/firmware/radarss/xwr12xx_xwr14xx_radarss.bin file indicates it is not a valid file to flash to IWR1443: 0xb55a03d1L
[18.12.2018, 14.45.17] [ERROR] Cortex_R4_0: !!! Aborting flashing of specified files!!!
[18.12.2018, 14.45.17] [INFO] Cortex_R4_0: Disconnecting from device on COM port COM18...
[18.12.2018, 14.45.17] [INFO] Cortex_R4_0: Flashing instance clean-up initiated...
[18.12.2018, 14.45.17] [INFO] Cortex_R4_0: Instance deinitialized!
I have tried SDK 1.02 2.01 and 3 but stil it is like this.
Best regards,
Mostafa