Hi,
I am reading the .dat file generated through the mmWave demo visualizer and using the parseTLV.py code to convert it into readable format. I have a few questions:
(1) What is the sampling rate?
(2) I see that I cannot increase the "Range Depth" beyond 10.47 m. Is this the max range of the sensor?
(3) What does the "range profile Y max = 2e6" mean?
(4) Can I get time-stamped samples from the .dat file generated?