Part Number: AWR1443BOOST
Other Parts Discussed in Thread: AWR1443, AWR1243BOOST, AWR1243, , UNIFLASH, IWR6843, MMWAVE-STUDIO
Hello,
what needs to be changed for DFP example to run on an AWR1443 ?
I received the following Messages :
=========== mmWaveLink Example Application ===========
rlComIfOpen Callback Called for Device Index [0]
Got 4 devices connected
Device 0: AR-DevPack-EVM-012 A , SN: FTQ3AW2A
Device 1: AR-DevPack-EVM-012 B , SN: FTQ3AW2B
Device 2: AR-DevPack-EVM-012 C , SN: FTQ3AW2C
Device 3: AR-DevPack-EVM-012 D , SN: FTQ3AW2D
SPI port opened (PortNum=0)
IRQ & I2C port opened (PortNum=1)
Board Control port opened (PortNum=2)
Generic GPIO port opened (PortNum=3)
rlDeviceEnable Callback is called by mmWaveLink for Device Index [0]
mmWave Device Power on failed for deviceMap 1 with error -8
=========== mmWaveLink Example Application execution Failed ===========
Thanks in advance and regards,
Metin