Other Parts Discussed in Thread: IWR1642
Hi all,
I am currently working in iwr1642 people counting demo application. I just want to know few details like ,
1. Does the posX and posY values from the sensor matches exactly the physical measurements of the target from the sensor.?
For example, the sensor is placed parallel to wall at 0 degrees with 15 degree tilt. A person standing at a distance of 3 meters directly away from the sensor . So the points we are getting will be (0,3)??
2. Does the height of sensor mount affects data points?
Example: At a height of 2.5meters from the ground, say, a person standing at one point gives (1.0,2.0) . If i increase the height of the mount from 2.5 m to 4 meters, will the person standing at the same point be (1.0,2.0) always??
Thanks in advance,
Ha An