Hi
I'm using the FDC1004 for liquid level sensing just as described in the TIDU736A reference design.
The FDC1004 is configured in differential mode measuring a LEVEL sensor, REFERENCE LIQUID sensor and REFERENCE ENVIRONMENT sensor. The three measurement channels are configured as follows:
MEAS1 = CIN1 (CHA) - CIN4 (CHB)
MEAS2 = CIN2 (CHA) - CIN4 (CHB)
MEAS3 = CIN3 (CHA) - CIN4 (CHB)
THe problem is that the measurements seem to have some offset (seen when measuring the air) and saturates before a the tank is filled.
Instead of just designing a new level sensing PCB (with a smaller sensing area), I would like to see what can be done in terms of adjusting gain and offset. But I'm a bit confused about how this can be done when the FDC1004 is operating in differential mode?
From what I can read from the datasheet the CAPDAC setting has no effect for a differential measurement.
What is left, is the OFFSET_CAL_CINx and GAIN_CAL_CINx (x=1,..,4) registers. How should these be interpreted?
Best Regards,
Andreas