This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1243BOOST: interface with Hercules launchpad

Part Number: AWR1243BOOST
Other Parts Discussed in Thread: LAUNCHXL2-570LC43, AWR1243

How to get raw data from AWR1243BOOST?

Is it possible to get raw data from AWR1243BOOST directly?

I do have access to Hercules Launchpad(LAUNCHXL2-570LC43) ... Does it help ?

  • Hi,

    The AWR1243BOOST can only send raw data out over an LVDS interface. You will need to use the DCA1000 EVM to capture this data.

    More information on this EVM is available here:
    www.ti.com/.../DCA1000EVM

    The Hercules Launchpad will not be able to acquire raw data from the AWR1243BOOST; it can however interface with the AWR1243 for control instead of a PC. Note that we do not provide any reference code or support for this configuration. Our supported control is from mmWaveStudio or mmWaveLink running on a PC.

    mmWaveStudio is available here: www.ti.com/.../MMWAVE-STUDIO
    mmWaveLink is available as part of the mmWaveDFP: www.ti.com/.../MMWAVE-DFP

    Best regards,
    Anand