Other Parts Discussed in Thread: TDC1000,
After START_MEAS is set, TRIGG pin goes high and never falls. Isn't it supposed to just output a pulse?
I measure Vreg=1.6V.
Clock is 16MHz.
thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
You mean with combined use with the tdc1000? I haven't gotten there yet, i just wanted to make sure tdc7200 worked first. TDC1000 works separately, producing the expected STOP pulses.
EDIT: I realized that in order for the TRIGG pin to go to 0 again, tdc7200 has to be connected to tdc1000. It works now.
thanks