Other Parts Discussed in Thread: PGA460
Hi,
I wanna use PGA460-Q1 in an application to detect an object upto 7m.
I want to connect multiple transducer of frequency 40KHz with single PGA460-Q1 to bring major area under detection range.
Is it possible to multiplex transducers in transformer drive mode.?
If yes, Please share sample schematic for reference.
If not possible, Then please suggest an alternative way to detect long range upto 7m. I am having a power supply of 12V DC.
Thank you.