Hi,
I am trying to run the example in the mmwave_automotive_toolbox_2_4_3.
After downloading the vitalSigns_16xx.bin, I execute VitalSignsRadar_Demo.
Then I get the following logs,
Configuration File Path is %s/n "E:/WORK/mmwave_automotive_toolbox_2_4_3/labs/lab0001-driver-vital-signs/vitalSigns_host/profiles/xwr1642_profile_VitalSigns_20fps_Front.cfg"
"sensorStop"
"flushCfg"
"dfeDataOutputMode 1"
"channelCfg 15 3 0"
"adcCfg 2 1"
"adcbufCfg -1 0 0 1 0"
"profileCfg 0 77 7 6 57 0 0 70 1 200 4000 0 0 48"
"chirpCfg 0 0 0 0 0 0 0 1"
"frameCfg 0 0 2 0 50 1 0"
"lowPower 0 1"
"guiMonitor 0 0 0 0 1"
"calibDcRangeSig -1 0 0 0 0"
"vitalSignsCfg 0.3 0.9 256 512 4 0.1 0.05 100000 300000"
"motionDetection 1 20 2.0 0"
"sensorStart"
""
"sensorStop"
"flushCfg"
"dfeDataOutputMode 1"
"channelCfg 15 3 0"
"adcCfg 2 1"
"adcbufCfg -1 0 0 1 0"
"profileCfg 0 77 7 6 57 0 0 70 1 200 4000 0 0 48"
"chirpCfg 0 0 0 0 0 0 0 1"
"frameCfg 0 0 2 0 50 1 0"
"lowPower 0 1"
"guiMonitor 0 0 0 0 1"
"calibDcRangeSig -1 0 0 0 0"
"vitalSignsCfg 0.3 0.9 256 512 4 0.1 0.05 100000 300000"
0.3
0.9
4
"motionDetection 1 20 2.0 0"
"sensorStart"
""
Chirp Duration in us is : 50
Chirp Bandwidth in kHz is : 3500
Maximum Range in Meters is : 8.57143
Range-FFT size is : 256
Range-Bin size is : 0.0334821
Range-Bin Start Index is : 8
Range-Bin End Index is : 26
Total Payload size from the UART is : 260
Padding Factor is : 9
Total Payload size from the UART is : 288
I can't get any signal, so I try to execute the those commands in the cfg file through putty.
mmwDemo:/>sensorStop
Done
mmwDemo:/>flushCfg
Done
mmwDemo:/>dfeDataOutputMode 1
Done
mmwDemo:/>channelCfg 15 3 0
Done
mmwDemo:/>adcCfg 2 1
Done
mmwDemo:/>adcbufCfg -1 0 0 1 0
Done
mmwDemo:/>profileCfg 0 77 7 6 57 0 0 70 1 100 2000 0 0 40
Done
mmwDemo:/>chirpCfg 0 0 0 0 0 0 0 1
Done
mmwDemo:/>frameCfg 0 0 2 0 50 1 0
Done
mmwDemo:/>lowPower 0 1
Done
mmwDemo:/>guiMonitor 0 0 0 0 1
Done
mmwDemo:/>calibDcRangeSig -1 0 0 0 0
Error: Number of averaged chirps is not power of two
Error -1
mmwDemo:/>vitalSignsCfg 0.1 0.7 256 320 1 0.1 0.05 300000 300000
Done
mmwDemo:/>motionDetection 1 20 0.04 0
Done
mmwDemo:/>sensorStart
Debug: Init Calibration Status = 0x7fe
Done
It seems the cfg is something wrong?