This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR1443BOOST: mm wave visualizer demo

Part Number: IWR1443BOOST

the evaluation module, before flashing the module with the required firmware, was connecting to the demo visualizer (i.e got recognized by the visualizer) however after the firmware was flashed to synchronize with the firmware that was used in the visualizer, the system is not recognizing the EVM module, and is now not responding to the command send config to mmwave device.

Thanks in advance for the help.

  • Hello Deveshwar,
    I hope you are following the steps provided in the mmWave SDK user guide to work with xWR1443 mmw demo and the visualizer.
    Other thing you need to take care about IWR1443 Silicon version, if it's ES 2.0 then you need to use SDK 1.2 else (ES3.0) then use SDK 2.0 version.
    Silicon +SDK version mismatch may cause this issue what you are facing.

    Regards,
    Jitendra