Other Parts Discussed in Thread: UNIFLASH, , MMWAVEICBOOST
So i recently bought a mmwaveicboost and IWR6843 antenna, but im having some trouble running the demo from the mmWave Demo Visualizer. I can flash the board using UniFlash, but when i change the SOP2 to open, restart the sensor, connect the demo visualizer with the correct COM ports, the demo only shows "waiting for data ..." even after i click "Send config to mmwave device". I've tried the "68xx - People counting demo" from the TI Resource explorer and again the same results (can flash the board but no communication after), using this demo the message is "Warning: Unsuccessful read: The specified amount of data was not returned within the Timeout period..".