Hello team,
I do have a few questions related to 60Ghz solutions:
1. does TI has a plan to release a device that supports 57-64 GHz in the future?
2. could you please advise what could be the power consumption (in mW) when the use case is to detect a person if he sits on a char with a duty cycle of 1min?
3. Do you have any technical material about horns and lenses?
4. when the IWR6843AOP should be released and if you can share the dimensions of antennas?
5. if you have any plan to release a lower cost device with less TX and RX with AOP for simple application such as distance measurements?
Thanks in advance
Best regards,
Shai