With the 9221, I've been looking at using the EEPROM and how it is being utilized. In the near future, I plan on developing a system based on the camera 8421, and the 9221, and I am a little confused on the EEPROM interface. Specifically, I am not certain of what is being stored on the EEPROM and in what format. Do you have any insight in this manner? Are the two different banks available via I2C stored into the EEPROM in a specific format?