Other Parts Discussed in Thread: IWR1443, TIDEP-0091, UNIFLASH
Hi,
Our application requires high accuracy and low power consumption.
For evaluation, I modified the High Accuracy Lab software to have a hard-coded chirp so that the IWR1443BOOST board (with IWR1443 ES3) can operate stand-alone.
Measuring the time from power-up of the board until the first range measurement is completed results in a duration of about 246 milliseconds.
This seems very long (too much power consumption), and longer than previous ES2 device.
Why is the time to the first measurement so long? (I understand that the boot sequence takes some time to read from the flash device and self-calibrate, but that does not explain > 200 ms duration).
Thanks,
-Chris